![Sugar centrifugation Sugar centrifugation](gemu-cdn2/anwendungsfaelle/bilder/64/IMGP7875_2018.jpg)
The Off stein plant of Südzucker AG uses continuously operating centrifuges supplied by the BMA mechanical engineering company (Braunschweigische Maschinenbauanstalt AG). These are used to separate the sugar and the mother liquor from the crystalline suspension. The sugar can then be dissolved or mashed in the centrifuge before it is fed into a further processing stage. In this process, the GEMÜ 550 globe valves reliably regulate the feed of wash water and steam into the centrifuges using the GEMÜ 1434 μPos positioner.