Applications in future markets
Above all, future means trust. Future markets trust the highly efficient products of GEMÜ. GEMÜ is thus a strong partner for its customers in the implementation of climate-neutral objectives. That can be seen in the use of its products, which are used in many different applications for state-of-the-art technologies.
![](fileadmin/user_upload/C3_1_350x300_photovoltaik-2.png)
Photovoltaic systems
The exploitation of CO2-neutral solar power also has an effect on the environmental balance of other sustainable technologies. Among other things, GEMÜ manufactures ultra pure, highly resistant valves that are used for the manufacture of photovoltaic panels in a specially constructed cleanroom plant in Emmen (Switzerland).
Wind power
Wind energy plays a decisive role in expanding renewable energies. Reliable wind power plants are now all the more important. The lubrication of turbines is a decisive process for a long service life and maintenance-free operation. GEMÜ valves are reliable plant components for minimizing complex and risky maintenance processes in this area
![](fileadmin/user_upload/C3_2_350x300_windkraft-7_09-21.jpg)
![](fileadmin/user_upload/350x300_mobilit%C3%A4t_01.png)
Mobility
In order to reduce the emission of CO2 when transporting people, automotive manufacturers are capitalizing on driver support through artificial intelligence and autonomous driving. A variety of MEMS (micro-electro-mechanical systems) are used to this end, which are included among the elementary components of modern vehicle safety and low emissions. The components are manufactured using ultra pure GEMÜ plastic valves.
![](fileadmin/user_upload/C3_4_350x300_Biotechnologie-11_09-21.jpg)
Recycling of agricultural waste
Methods of recycling liquid manure and digestate from biogas plants are important future technologies. They save our agricultural areas from over-fertilization, thus protecting our bodies of water and feeding valuable raw materials back into the economic cycle. GEMÜ valve systems take on important process steps such as media dosing in recycling facilities for agricultural waste.
Water treatment
In order to protect not only ourselves but also our environment from contaminated water, the water treatment plants of the manufacturing industry, which can be reliably operated with GEMÜ equipment, are also of great significance.
They differ here in capacity and size. A special feature is that they don't emit any CO2 when stationary, which makes them particularly sustainable.
![](fileadmin/user_upload/C3_5_350x300_Wasseraufbereitung.png)
![](fileadmin/user_upload/C3_6_350x300_Batterien-10_09-21.jpg)
Batteries
Batteries are electrochemical energy stores. The most frequent area of use is currently lithium-ion accumulators, which are used both in small smartphones and for electromobility. They differ here in capacity and size. A special feature is that they don't emit any CO2 when stationary, which makes them particularly sustainable. GEMÜ supports this technology with products specially for battery production.