![](fileadmin/user_upload/Aktuelles/News/2021/UL_certification_GEMUE_1235_1236_1436_eco_200px.jpg)
GEMÜ, the valve specialist, has had a further three of its intelligent automation components certified with UL approval: The GEMÜ 1235 and GEMÜ 1236 electrical position indicators and the GEMÜ 1436 eco cPos positioner.
The UL certification mark is valid for the USA and Canada. It is practically a prerequisite for all machines and plant components that are used or exported there.
GEMÜ 1235 and GEMÜ 1236 electrical position indicators
The GEMÜ 1235 and GEMÜ 1236 electrical position indicators are characterized by their compact and simple design, which still offers state-of-the-art functions. They feature the conventional discrete indication of the process valve position (closed or open) as well as IO-Link communication. The products are available in plastic and stainless steel.
GEMÜ 1436 eco cPos positioner
The GEMÜ 1436 eco cPos positioner is very versatile in use. The electronic system has been reduced to the core functions. Together with the quick commissioning function (speed-AP), this makes for a positioner that is incredibly easy to use and suitable for control tasks with basic requirements.