Focus on reliable and intelligent processes: GEMÜ CONEXO
Video only available in German!
GEMÜ focused entirely on the motto "Process reliability" at ACHEMA 2015. One example of this is CONEXO – the future of intelligent valve technology. This involves linking valve components which have an RFID chip to an IT infrastructure, comprising the CONEXO APP and the CONEXO Portal.
Every valve and every relevant valve component, such as the body, actuator or diaphragm, can be clearly traced using serialization and read off at any time in the system using the RFID reader – the CONEXO PEN. The CONEXO APP, which can be installed on mobile devices, will not only simplify and improve the "Installation qualification" process; it will also make the maintenance process much more reliable and easier to document in the future. The app actively guides the maintenance technician through the maintenance schedule and directly provides him with all the information assigned to the valve, such as test reports, testing documentation and maintenance histories. This will optimize the maintenance processes in the systems and thus make a significant contribution to increasing process reliability.
The film will provide an initial insight into the current project.